From the "%DIR_PATH%\SOFTWARE\" folder, launch the following command:
The following contents appear in the Command Prompt window and in the debug UART interface.
When the three tests are a pass, indicated by a āPā as shown above, the connection between the two devices is confirmed.
If the test is stuck, the only way to return to a valid state is to perform a hardware reset by forcing the NRST signal to ground.