The debugWIRE OCD is drastically downscaled when compared to the Microchip megaAVR (JTAG) OCD. This means that it does not have any Program Counter breakpoint comparators available to the user for debugging purposes. One such comparator does exist for purposes of run-to-cursor and single-stepping operations, but additional user breakpoints are not supported in hardware.
Instead, the debugger must make use of the AVR
BREAK
instruction. This instruction can be placed in FLASH, and when loaded for
execution, it will cause the AVR CPU to enter Stopped mode. To support breakpoints during
debugging, the debugger must insert a BREAK
instruction into FLASH at the
point at which the users request a breakpoint. The original instruction must be cached for
later replacement. When single-stepping over a BREAK
instruction, the
debugger has to execute the original cached instruction to preserve program behavior. In
extreme cases, the BREAK has to be removed from FLASH and replaced later. All these
scenarios can cause apparent delays when single-stepping from breakpoints, which will be
exacerbated when the target clock frequency is very low.
It is thus recommended to observe the following guidelines, where possible:
Always run the target at as high a frequency as possible during debugging. The debugWIRE physical interface is clocked from the target clock.
Try to minimize the number of breakpoint additions and removals, as each one requires a FLASH page to be replaced on the target
Try to add or remove a small number of breakpoints at a time, to minimize the number of FLASH page write operations
If possible, avoid placing breakpoints on double-word instructions