CRYPTO_AHB_SLAVE |
Bus |
AHB-Lite slave interface, which is used
for control, and primary data input and output. |
CRYPTO_AHB_MASTER |
Bus |
AHB-Lite master DMA interface, which
may optionally be used for data input and output. |
CRYPTO_HCLK |
Input |
AHB bus clock. |
CRYPTO_HRESETN |
Input |
The reset signal, CRYPTO_HRESETN, is
active low, synchronous, and is sampled on the rising edge of the clock.
Asserts the functional reset of the User Cryptoprocessor block and
zeroizes all the internal RAM and registers as PURGE signal. It is
necessary to assert this signal for a minimum of two clock cycles to
reset the core. |
CRYPTO_GO_F2M |
Input |
External execution initiation input
when the User Cryptoprocessor operates in the standalone configuration
without a host processor connected to the bus interface. Asserting the
GO signal causes the User Cryptoprocessor to initiate execution. During
execution, the status of the User Cryptoprocessor is reflected by the
BUSY and DLL_LOCK ports. This signal must be tied low when the User
Cryptoprocessor is used as a co-processor. |
CRYPTO_PURGE_F2M |
Input |
When the signal is set to '1', it
initializes the Zeroization of User Cryptoprocessor internal RAM and
registers. For normal operation, this signal must be tied low. The PURGE
input is level sensitive, and if the PURGE pin is still asserted when a
purge operation completes, another purge operation is initiated. |
CRYPTO_STALL_F2M |
Input |
Stalls the User Cryptoprocessor for a
clock cycle, to introduce variance in the external signatures. The STALL
input is expected to be generated by a LFSR circuit in the fabric and
asserted randomly for a single cycle to achieve the required stall
rates. The STALL input must not be asserted until at least three clock
cycles after the HRESETN is de-asserted and the DLL has indicated LOCK
for three cycles. |
CRYPTO_ALARM_M2F |
Output |
Asserted to indicate an uncorrectable
memory error condition. An uncorrectable memory error causes the Crypto
core to perform a reset and purge. This reset terminates any in-progress
operation. For most CAL operations, the CALPKTrfRes() function is used
to complete the operation and generates a hardware fault code in the
event of an alarm. |
CRYPTO_BUSERROR_M2F |
Output |
Asserted when a HRESP response error is
detected by the User Cryptoprocessor AHB master. When set, a reset is
required to clear. |
CRYPTO_BUSY_M2F |
Output |
Execution status signal |
CRYPTO_COMPLETE_M2F |
Output |
Active high signal, asserted on raising
edge of CRYPTO_HCLK to indicate that the User Cryptoprocessor has
completed an operation. This signal can be connected to the host
microprocessor as an interrupt request signal, enabling the User
Cryptoprocessor to interrupt the processor when it completes an
operation. |
CRYPTO_DLL_LOCK_M2F |
Output |
DLL lock status |
CRYPTO_MESH_CLEAR_F2M |
Input |
Crypto Mesh error clear should be
asserted for at least 5 ns |
CRYPTO_MESH_ERROR_M2F |
Output |
Indicates that the security mesh
detected an error because of wires are cut or shorted. When set, stays
set until cleared. |
Cryptoprocessor
Ownership Handshake Interface |
CRYPTO_REQUEST_F2M |
Input |
Fabric request or is using the
Cryptoprocessor |
CRYPTO_MSS_REQUEST_M2F |
Output |
MSS request or is using the
Cryptoprocessor |
CRYPTO_RELEASE_F2M |
Input |
Fabric released the
Cryptoprocessor |
CRYPTO_MSS_RELEASE_M2F |
Output |
MSS released the
Cryptoprocessor |
CRYPTO_OWNER_M2F |
Output |
Indicates that the Fabric owns the
Cryptoprocessor and the fabric interface is enabled |
CRYPTO_MSS_OWNER_M2F |
Output |
Indicates that the MSS owns the
Cryptoprocessor and the fabric interface is disabled |
CRYPTO_REQUEST_F2M |
Input |
Fabric request or is using the
Cryptoprocessor |
CRYPTO_MSS_REQUEST_M2F |
Output |
MSS request or is using the
Cryptoprocessor |
Cryptoprocessor
Streaming Interface |
CRYPTO_XWDATA_F2M |
Input |
Transfer in data |
CRYPTO_XWADDR_M2F |
Output |
Transfer in data address output |
CRYPTO_XENABLE_F2M |
Input |
Transfer in data request |
CRYPTO_XINACCEPT_M2F |
Output |
Transfer in data accept |
CRYPTO_XRDATA_M2F |
Output |
Transfer out data |
CRYPTO_XRADDR_M2F |
Output |
Transfer out data address
output |
CRYPTO_XVALIDOUT_M2F |
Output |
Transfer out data valid output |
CRYPTO_XOUTACK_F2M |
Input |
Transfer out data
acknowledgment |