If external pad is selected as input clock, code is now generated with the frequency added by the user. An issue with the current release is that the frequency is displayed as 0 in the clock view, but the generated code have the correct frequency.
Pinmux is reset correctly when pin mode is changed a second time.
In some cases START fails to add 2 or more instances of a driver even if allowed. A message is now displayed suggesting adding instances one by one.
Frequency Hop module is updated to support 256 channel. The issue related to "Frequency Hop module may not work as intended" is solved.