Issue #4146: Line continuation doesn't work in macro calls
The following program illustrates this issue.
.macro m ldi @0, @1 .endm m r16,\ 0
This is not a problem with preprocessor macros
(#define
).
Missing newline at end of file
AVRASM2 has some issues if the last line in a source file is missing a newline: Error messages may refer to wrong filename/line number if the error is in the last line of the included files, and in some cases syntax errors may result. Beware that the Atmel Studio editor will not append a missing newline at the end of a source file automatically.
Increment/decrement operators
Increment/decrement operators (++/--) are recognized by the assembler and may cause surprises, e.g.:
symbol--1
will cause a syntax error, write symbol -
-1
if the intention is to subtract -1.
This behavior is consistent with C compilers. The ++/-- operators are not useful in the current assembler, but are reserved for future use.
Forward references in conditionals
Using a forward reference in an assembler conditional may cause surprises, and in some cases is not allowed. Example:
.org LARGEBOOTSTART ; the following sets up RAMPZ:Z to point to a FLASH data object, typically ; for use with ELPM. ldi ZL, low (cmdtable * 2) ldi ZH, high (cmdtable * 2) .if ((cmdtable * 2) > 65535) ldi r16, 1 sts RAMPZ, r16 .endif ; more code follows here cmdtable: .db "foo", 0x0
The reason for this is that the outcome of the conditional will influence the value of the forward referenced label, which in turn may affect the outcome of the conditional, and so on.
The following is allowed:
.ifdef FOO nop ; some code here .endif rjmp label ; more code here .equ FOO = 100 label: nop
In this example FOO is not defined at the point it is used in a conditional. The use of .ifdef in this situation is allowed, and the conditional is false. However, the pattern shown above is not recommended because the programmer's intention is not clear. The form is intended to allow common constructs like this:
; Define FOO if it is not already defined. .ifndef FOO .equ FOO = 0x100 .endif
Up to and including AVRASM 2.0.30, these situations were not always properly detected, causing incomprehensible error messages. Starting with 2.0.31, explicit error messages are given.
Note that with preprocessor conditionals (#if/#ifdef
),
the situation is always well-defined, preprocessor symbols are always undefined until the
definition is seen, and this kind of error will never occur.
Error messages
Sometimes error messages may be hard to understand. Typically, a simple typo in some instances may produce error messages like this:
myfile.asm(30): error: syntax error, unexpected FOO
where FOO represents some incomprehensible gibberish. The referenced filename/line number is correct, however.
defined incorrectly treated as an assembler keyword
The keyword defined is recognized in all contexts. It should only be recognized in conditionals. This prevents defined to be used as a user symbol like a label, etc. On the other hand, it allows for constructs like '.dw foo = defined(bar)', which it shouldn't. Note that the preprocessor and assembler have separate implementations of defined. The exact behavior of defined currently (from 2.1.5) is:
The preprocessor 'defined' keyword only relates to symbols defined
with #define
, and correctly does this only in preprocessor
conditionals (#if/#elif
).
In all remaining code, the assembler's notion of defined is
used, the correct behavior would be to only recognize it in assembler conditionals
(.if/.elif
).
Preprocessor issues
The preprocessor will not detect invalid preprocessor directives inside a false conditional. This may lead to surprises with typos like this:
#if __ATmega8__ //... #elseif __ATmega16__ //WRONG, the correct directive is #elif // This will go undetected if __ATmega8__ is false //... #else // when __ATmega8__ is false this section will be assembled even if // __ATmega16__ is true. #endif
It is debatable if this is a bug, the behavior is consistent with the C preprocessor.
Issue #3361: The preprocessor incorrectly allows additional text after directives, which may cause surprises, e.g., #endif #endif will be interpreted as a single #endif directive, without any error or warning message.
#define TEST \
.IF val \
.DW 0 \
.ELSE \
.DW 1 \
.ENDIF
The reason for this is that assembler conditionals must appear on a separate line,
and a preprocessor macro like the above is concatenated into a single line.