Definition: This function un-registers a file to the PDS. This makes the data stored in the NVM invalid and any operation on this file ID will be invalid after this point.
Syntax
PdsStatus_t PDS_UnRegFile(PdsFileItemIdx_t argFileId);
Input Parameters
Parameter Name |
Parameter Type |
Description |
---|---|---|
argFileId |
PdsFileItemIdx_t |
PDS file ID of the item |
Return Type and Values
Parameter Name |
Parameter Type |
Description |
---|---|---|
|
ENUM |
PDS status codes. Definition available in
|
Return Value |
Reason |
---|---|
PDS_OK |
PDS operation is success |
PDS_INVALID_FILE_IDX |
File ID in the argument is not valid one |
API Type – Synchronous