Definition: This function transmits a continuous wave. This API uses radio
parameters (such as Frequency, Modulation, Spreading factor and so on) stored in TAL
data base to transmit the continuous wave. Radio parameters can be configured using
RADIO_SetAttr
API described in RADIO_SetAttr. If user did not configure any parameters, this API will use default parameters
stored in data base. All default values for the radio layer are given in the Radio/TAL Attributes.
Syntax
RadioError_t RADIO_TransmitCW(void);
Input Parameters
<None>
Return Type and Values
Parameter Name |
Parameter Type |
Description |
---|---|---|
|
ENUM |
Enumerated values containing all return types from radio layer |
Return Value |
Reason |
---|---|
ERR_RADIO_BUSY |
Radio is not in IDLE state |
ERR_NONE |
Radio in IDLE state and starts the continuous transmission |
API Type – Synchronous