Definition: This function is used to read a byte of data from the radio register.
Syntax
Uint8_t RADIO_RegisterRead(uint8_t reg)
Input Parameters
Parameters Name |
Parameter Type |
Description |
---|---|---|
reg |
uint8_t |
Register address to be read |
Return Type and Values
Parameters Name |
Parameter Type |
Description |
---|---|---|
Uint8_t |
8-bit unsigned integer |
Value read from the radio register |
API Type - Synchronous