Definition: This function is called by the stack to indicate HAL for resetting the Rfctrl GPIO pins to their inactive state. Based on RFCTRL1 and RFCTRL2 values, different GPIOs will be controlled.
Syntax
void HAL_DisableRFCtrl(RFCtrl1_t RFCtrl1, RFCtrl2_t RFCtrl2)
Input Parameters
Parameters Name |
Parameter Type |
Description |
---|---|---|
RFCtrl1 |
ENUM |
RF Control 1 indicates the FREQUENCY band (Higher UHF or Lower UHF) or PA Boost enabled. RFO_LF = 0 RFO_HF = 1 PA_BOOST = 2 |
RFCtrl2 |
ENUM |
RF Control 2 indicates Transmit or Receive path RX = 0 TX = 1 |
Return Types and Values
<void>
API Type - Synchronous