Definition: This function registers a file to the PDS.
Syntax
PdsStatus_t PDS_RegFile(PdsFileItemIdx_t argFileId, PdsFileMarks_t argFileMarks);
Input Parameters
Parameter Names |
Parameter Types |
Description |
---|---|---|
argFileId |
PdsFileItemIdx_t |
PDS file ID of the item. |
argFileMarks |
PdsFileMarks_t |
This structure contains details about number of items in file, RAM address for each item and size of each item in a list form. This will be stored in PDS and used to retrieve data during PDS operations. |
Return Type and Values
Parameter Name |
Parameter Type |
Description |
---|---|---|
|
ENUM |
PDS status codes. Definition available in
|
Return Value |
Reason |
---|---|
PDS_OK |
PDS operation is success |
PDS_INVALID_FILE_IDX |
File ID in the argument is not valid one |
API Type – Synchronous