Definition: This function is used to write a byte of data to the radio register
Syntax
void RADIO_RegisterWrite(uint8_t reg, uint8_t value)
Input Parameters
Parameter Names |
Parameter Type |
Description |
---|---|---|
reg |
uint8_t |
Register address to be written |
value |
uint8_t |
Value to be written into the radio register |
Return Type and Values
<void>
API Type - Synchronous