Module | Feature | Item No. | Issue Summary | Affected Revisions | |
---|---|---|---|---|---|
A2 | A3 | ||||
Analog-to-Digital Converter (ADC) | ADC Conversion | ADC Conversion | Delay of one instruction cycle required prior to setting the ADGO bit when using ADCRC as the ADCC clock source. | X | |
ADCRC Oscillator Operation in Sleep |
ADCRC Oscillator Operation in Sleep | The ADCRC oscillator does not stop after conversion is complete in Sleep mode. | X | X | |
ADC Conversion with FVR | ADCRC Oscillator Operation in Sleep | Using FVR as the ADC positive voltage reference can cause missing codes. | X | X | |
ADC conversion with FOSC as clock | ADCRC Oscillator Operation in Sleep | The ADGO bit remains set when using FOSC as clock source with clock divider. | X | X | |
ADC operation in Burst Average mode | ADCC Burst Average Mode | The ADCNT register does not increment past ’0b1’ in Burst Average mode with double sampling enabled. | X | X | |
Double Sample Conversions | Double Sample Conversions | An unexpected acquisition time is added between the first and second conversions. | X | X | |
ADC Acquisition Time | ADC Conversion Acquisition Time in Sleep (ADCC) | Conversion during SLEEP mode when ADACQ=0 affects results on values in the upper half of the 10-bit range. The analog input is disconnected for 3-4 uS and the first bit of the result becomes zero. | X | X | |
ADC Short in Precharge State | ADC Short in Pre-Charge State | ADC shorts briefly in pre-charge state when the corresponding analog pin is selected as an output. | X | X | |
PIC18 Debug Executive | Data Write Match Breakpoints | Data Write Match Breakpoints | Data write match breakpoints do not work when used on a location GSR space. | X | |
Single Step Function (SSTEP) | Single Step function does not execute at SW Breakpoint. | Single Step function does not execute at SW Breakpoint. | X | X | |
PIC18 Core | TBLRD | TBLRD Requires NVMREG Value to Point to Appropriate Memory | TBLRD requires NVMREG value to point to appropriate memory. | X | |
Program Flash Memory (PFM) | Endurance of PFM Cell | Endurance of PFM is Lower than Specified | Endurance of the PFM cell is lower than specified. | X | X |
Back to Back Writes | PFM Back to Back Writes | Repetitive writes may cause write/erase failures. | X | X | |
MSSP | SMBus 2.0 Voltage Level | SMBus 2.0 Voltage Level | Input low-voltage threshold level is dependent on VDD. | X | X |
SPI | MSSP SPI Client Mode | SSPBUF may become corrupted | X | X | |
I2C | SMBus 2.0 Voltage Level | Acknowledge failure on LF devices only | X | ||
Electrical Specifications | Min VDD Specification | Min VDD Specification (LF Devies Only) |
VDDMIN specifications are changed for LF devices only for -40°C and 0°C. |
X | |
FVR Specification | FVR - Fixed Voltage Reference | FVR specifications require use above -20°C. | X | X | |
Analog to Digital Converter | ADC - Analog-to-Digital Converter | ADC offset error specification is +/- 3.0 LSb. | X | X | |
Timer0 | Clock Source | Synchronous mode | TMR0 does not function properly in Sync mode | X | X |
Windowed Watchdog Timer | WWDT operation in Doze mode | Window Operation in Doze Mode | Erroneous window violation error occurs in Doze mode. | X | X |
NVM | NVMERR bit operation | NVMERR | NVMERR bit is set incorrectly due to specific Reset events. | X | X |
SMT | Reset bit | Reset Bit | Module stops working if RST is set while prescaler setting is not zero | X | X |
Enhanced Universal Synchronous Asynchronous Receiver Transmitter (EUSART) | Transmit mode | Double Byte Transmit | Possible duplicate byte transmitted | X | X |
Capture/Compare/PWM Module (CCP) | PWM mode | Wrong Duty Cycle for CCP Module | Duty cycle values are incorrect | X | X |
In-Circuit Serial Programming™ | Low-Voltage Programming | Low-Voltage Programming Not Possible | Low-Voltage Programming is not possible when VDD is below BORV while BOR is enabled | X | X |
Note: Only those issues
indicated in the last column apply to the current silicon
revision.
|