When using the ADCRC as the clock source for ADCC, there is a delay of
one instruction cycle between the user setting the ADGO bit and being able to read
it set. This can lead to a false conversion complete scenario (i.e., ADGO being
cleared), depending if the user code has a bit clear test BTFSC
instruction on the ADGO bit, immediately after setting the ADGO bit. See code
example below.
BSF ADCON0, ADGO ; Start conversion
BTSFC ADCON0, ADGO ; Is conversion done?
GOTO $-1 ; No, test again
Add a NOP
instruction after setting the ADGO bit and
before testing the bit for completion of conversion. See code example below.
BSF ADCON0, ADGO ; Start conversion
NOP
BTSFC ADCON0, ADGO ; Is conversion done?
GOTO $-1 ; No, test again
A2 | A3 |
X |