The following section provides a set of terms used to discuss configuration
options. The terms are arranged alphabetically.
- Term
- Description
- AES Key
- Slot can be used as a key source for
AES
commands. The AES key is 128 bits in width for the ATECC608A-TFLXTLS.
- Always Write
- Slot can be written in the clear with the
Write
command.
- Clear Read
- Slot is considered public (non-secret) and its contents can be read in the
clear with the
Read
command.
- ECDH
- Elliptic Curve Diffie Hellman. Private key can be used with the
ECDH
command.
- Encrypted Write
- Slot can only be written using an encrypted write based on the
write key specified.
- Ext Sign
- Private key can be used to sign external (arbitrary) messages.
- Int Sign
- Private key can be used to sign internal messages generated by the
GenKey
or GenDig
commands. Used to
attest to the device's internal keys and configuration.
- Lockable
- Slot can be locked at some point in the future. Once locked, the
slot contents cannot be changed (read/use only).
- No Read
- Slot is considered secret and its contents cannot be read with the
Read
command. Private keys and symmetric secrets should
always be configured as No Read.
- No Write
- Slot cannot be changed with the
Write
command.
- Permanent
- Private key is permanent/unchangeable. It is internally generated during
factory provisioning.
- Updatable
- Private key can be overwritten later with a new, random,
internally-generated private key. Its initial value is internally generated
during factory provisioning.
- Validated
- Public key can only be used with the
Verify
command once it has been validated by the parent public key.