GenDig - Config

Data from the Configuration zone can be included in the GenDig calculation. Data are always included in 32-byte blocks and only one block may be included on any given GenDig calculation. The Nonce command must be run prior to the first GenDig command to load a value into TempKey. Subsequent GenDig commands will use the value stored in TempKey from the previous GenDig operation.
Table 1. Input Parameters GenDig Config

Opcode
(1 Byte)

Mode
(1 Byte)

KeyID(1)
(2 Bytes)

Data
(0 Bytes)

Description
0x15 0x00 0x00 00 Use Configuration Block 0
0x00 01 Use Configuration Block 1
0x00 02 Use Configuration Block
0x00 03 Use Configuration Block 3
Note:
  1. 1.KeyId specifies the Configuration zone block to be used in the TempKey Calculation.
Table 2. Output Response - GenDig Config
Name Size Description
Response 1 byte

0x00 - If successful.

Error code - If the command fails.

Notes: Flag Bits
  1. 1.TempKey.Valid flag will be set to 1 if successful, otherwise it is 0.
  2. 2.TempKey.GenDigData will be set to 0.
Table 3. TempKey Calculation - GenDig Config
 

32 bytes
1 byte
1 byte
2 bytes
1 byte
2 bytes
25 bytes
32 bytes

Configuration Zone Block
Opcode = 0x15
Mode = 0x00
KeyID[0:1] = 0x0[block] 0x00
SN[8] = 0x01
SN[0:1] = 0x01 0x23
All Zeros
TempKey.Value