Nonce
command must be run prior to the first
GenDig
command to load a value into TempKey. Subsequent
GenDig
commands will use the value from the previous GenDig
operation.
Opcode |
Mode |
KeyID(1) |
Data |
Description |
---|---|---|---|---|
0x15 | 0x01 | 0x00 00 | — | Use OTP Block 0 as the KeyID |
0x00 01 | — | Use OTP Block 1 as the KeyID |
Name | Size | Description |
---|---|---|
Response | 1 byte |
0x00 - If successful. Error code - If the command fails. |
32 bytes |
OTP Zone Block |