If the MPLAB ICE 4 In-Circuit
Emulator and MPLAB X IDE are not communicating with each other:
- 1.Unplug and then plug in the debugger.
- 2.Reconnect to the debugger.
- 3.Try the operation again. It is possible the error was a one-time event.
- 4.The version of a pack (DPF/TP) installed in MPLAB X IDE may
be incorrect for the target device. See MPLAB X IDE
documentation for information on how to install updated packs.
- 5.There may be an issue with the computer USB port. See section USB Port Communication
Error Actions.