Data capture provides streaming data from a device.
To set up data capture:
- 1.Build the project (In the Projects
window, right click on the project name and select “Build”). The project must be
built to see the available symbols: Project Properties>Loading, check
“Load symbols when programming or building for production (slows process)”.
- 2.Select Window>Debugging>Watches to open the Watches window.
- 3.Right click in the window and select “New Watch”. Select the symbol or SFR wish to
watch in the New Watch window. Click OK.
- 4.Begin a debug session . View
data in Watches window.