Set up emulator options on the emulator property pages of the Project Properties
dialog.
- 1.Open the Project Properties dialog by doing one of the following:
- a.Click the project name in the Projects window, select File>Project
Properties.
- b.Right click the project name in the Projects window, select
“Properties”.
- 2.Under “Categories”, click on “ICE 4”
- 3.Select property pages from “Options
categories”. Click on an option to see its description in the text box below it.
Click to the right of an option to change it.
Note: Options displayed may be
different for different devices.
Figure 1. Project Properties - ICE 4 Options