Use the Project Properties dialog to select or switch emulators for a project. To switch
you must have more than one MPLAB® ICE 4 In-Circuit
Emulator connected to your computer. MPLAB X IDE will differentiate between the two by displaying two
different serial numbers.
To select or change the emulator used for a project:
- 1.Open the Project Properties dialog by doing one of the following:
- a.Click on the project name in the Projects window and select
File>Project Properties.
- b.Right click on the project name in the Projects window and select
“Properties”.
- 2.Under “Categories”, click on “Conf: [default]”
- 3.Under “Hardware Tools”, find “ICE 4” and click on a serial number (SN) to select an
emulator for use in the project.