Now see how
components placed on a dashboard in Data Visualizer can be hooked up to variables in the
application, and how the dashboard can thus interact with the application at
run-time.
Instead of a
predefined interval of 1000 USB sync pulses (1 second), add a variable compare reference
to the original code.
Todo: Modify ui.c to include a LED blinker
in the ui_process() handler as shown here.
volatile uint32_t frame_comparator =100;volatile uint32_t frames_received =0;voidui_process(uint16_t framenumber){
frames_received++;if(frames_received >= frame_comparator){LED_Toggle(LED_0_PIN);
frames_received =0;}}
Todo: - Build the project/solution
(F7)
- Launch a debug session using
Start Debugging and Break (Alt + F5)
- Find the location of the
variable uint32_t frame_comparator
Todo: - Open Data Visualizer
- Connect
- Add the location of the
frame_comparator in the Code Profiling Configuration window
A Data Visualizer dashboard can now be made with controls which manipulate the
value of this variable.