To be able to work through this example, the following is required:
- Host computer with Atmel Studio 7 (or
later) installed (Data Visualizer is included)
- Microchip Power Debugger Kit (cabling included)
- Microchip ATSAM L21 Xplained Pro Kit,
or similar target board with USB device connector, external programming header, and
current measurement header
Tip: The SAM L21 Xplained Pro
also has integrated on-board current measurement features, but these will not be used in
this use case.