To display information about the breakpoints commands available in MDB, type
help breakpoints
. The following table provides additional
information for this class of commands
Command | Description |
---|---|
Break | Sets a breakpoint at the specified source line number. Command format:
Example:
|
Sets a breakpoint at an absolute address. Command format:
Example:
MDB assigns a
breakpoint number and returns: |
|
Sets a breakpoint at the beginning of the function. Command format:
Example:
|
|
Delete | Deletes a breakpoint – if no argument is specified, this
deletes all breakpoints. You can abbreviate this command
as Command format:
The
breakpoint number is generated by MDB for the Examples:
|
Halt | Stops the debugger program. |
Watch | Sets a data breakpoint at the specified memory address,
variable name, or an SFR (special function register). Command format:
Examples:
MDB will assign and
return the watchpoint number, for example: |