If programming and debugging needs to be done frequently or multiple times, run the test by running a command file. This is more efficient than entering the commands repeatedly. Put all the commands in a file and run the MDB using this command file in the Command Prompt, for example:
C:\Program Files\Microchip\MPLABX\vn.nn\mplab_ide\bin>mdb.bat
<commandfile.txt>
The following is an example of a command file:
C:\MDB-SIMCommand_Target.txt
A line starting with # means that it is a comment. A Sleep command should be added to make sure the MDB has enough time to finish the previous command before it executes the next command. The MDB will run all the commands in the command file sequentially.
Creating a Printable Log File
Redirecting output to a file is a general option that can be executed from the command prompt and is not specific to the MDB batch file. Redirecting output to a printable text file can be more useful for examining errors than looking at the Command Prompt window.
To create a printable file, open the MDB.bat file, and modify it by adding
>>%mplabx_dir%\bin\mdblog.txt
at the end of the batch file. This
instructs the batch file to create the mdblog.txt file, which can be printed.