Use the following commands to debug a device.
Reset
Set a breakpoint by source-line-number using the command:
Break
filename: linenumber
For example: Break
main.c:53
Set a breakpoint at an absolute address using command:
Break *address
For example: Break
*0x108
Set a watchpoint by specifying an address and the type of watch using the command:
Watch address breakontype
For example:
Watch 0xa0007ff0 R
or
Watch address
breakontype[:value] [passcount]
For example: Watch
0xa0007ff0 R:0xf 1
Delete [breakpoint
number]
If no argument is specified in this command, it will delete all breakpoints.