For a list of all commands within a particular class, type help
followed
by the class name. The help
command can also be abbreviated to
h
. See the following tables for information about each class of
commands.
For documentation on a particular command, type help [command or
class of commands]
to display information about the command. For example,
if you type:help breakpoints
or h Breakpoints
the MDB
displays information about the break, watch, delete and halt commands.
The following sections provide information on commands.