When switching between tri-state ({DDxn, PORTxn} = 0b00) and output high ({DDxn, PORTxn} = 0b11), an intermediate state with either pull-up enabled {DDxn, PORTxn} = 0b01) or output low ({DDxn, PORTxn} = 0b10) must occur. Normally, the pull-up enabled state is fully acceptable, as a high-impedance environment will not notice the difference between a strong high driver and a pull-up. If this is not the case, the PUD bit in the MCUCR Register can be set to disable all pull-ups in all ports.
Switching between input with pull-up and output low generates the same problem. The user must use either the tri-state ({DDxn, PORTxn} = 0b00) or the output high state ({DDxn, PORTxn} = 0b11) as an intermediate step.
The following table summarizes the control signals for the pin value.
DDxn | PORTxn | PUD (in MCUCR) | I/O | Pull-up | Comment |
---|---|---|---|---|---|
0 | 0 | X | Input | No | Tri-state (Hi-Z) |
0 | 1 | 0 | Input | Yes | Pxn will source current if ext. pulled low |
0 | 1 | 1 | Input | No | Tri-state (Hi-Z) |
1 | 0 | X | Output | No | Output Low (Sink) |
1 | 1 | X | Output | No | Output High (Source) |