The Flash is organized in pages as number
of Words in a Page and number of Pages in the Flash. When programming the Flash, the
program data is latched into a page buffer. This allows one page of program data to be
programmed simultaneously. The following procedure describes how to program the entire
Flash memory:
Step A. Load Command “Write
Flash”
- 1.Set XA1, XA0 to “10”. This enables
command loading.
- 2.Set BS1 to “0”.
- 3.Set DATA to “0001 0000”. This is the
command for Write Flash.
- 4.Give XTAL1 a positive pulse. This
loads the command.
Step B. Load Address Low Byte
- 1.Set XA1, XA0 to “00”. This enables
address loading.
- 2.Set BS1 to “0”. This selects low
address.
- 3.Set DATA = Address low byte (0x00 -
0xFF).
- 4.Give XTAL1 a positive pulse. This
loads the address low byte.
Step C. Load Data Low Byte
- 1.Set XA1, XA0 to “01”. This enables
data loading.
- 2.Set DATA = Data low byte (0x00 -
0xFF).
- 3.Give XTAL1 a positive pulse. This
loads the data byte.
Step D. Load Data High Byte
- 1.Set BS1 to “1”. This selects high
data byte.
- 2.Set XA1, XA0 to “01”. This enables
data loading.
- 3.Set DATA = Data high byte (0x00 -
0xFF).
- 4.Give XTAL1 a positive pulse. This
loads the data byte.
Step E. Latch Data
- 1.Set BS1 to “1”. This selects high
data byte.
- 2.Give PAGEL a positive pulse. This
latches the data bytes. (Please refer to the figure, Programming the Flash Waveforms,
in this section for signal waveforms)
Step F. Repeat B Through E Until the
Entire Buffer Is Filled or Until All Data Within the Page Is Loaded
While the lower bits in the address are
mapped to words within the page, the higher bits address the pages within the FLASH.
This is illustrated in the following figure, Addressing the Flash Which is Organized in
Pages, in this section. Note that if less than eight bits are required to address words
in the page (pagesize < 256), the most significant bit(s) in the address low byte are
used to address the page when performing a Page Write.
Step G. Load Address High
Byte
- 1.Set XA1, XA0 to “00”. This enables
address loading.
- 2.Set BS1 to “1”. This selects high
address.
- 3.Set DATA = Address high byte (0x00 -
0xFF).
- 4.Give XTAL1 a positive pulse. This
loads the address high byte.
Step H. Program Page
- 1.Give WR a
negative pulse. This starts programming of the entire page of data.
RDY/BSY goes low.
- 2.Wait until
RDY/BSY goes high (Please refer to the figure,
Programming the Flash Waveforms, in this section for signal waveforms).
Step I. Repeat B Through H Until the
Entire Flash Is Programmed or Until All Data Has Been Programmed
Step J. End Page Programming
- 1.1. Set XA1, XA0 to “10”. This
enables command loading.
- 2.Set DATA to “0000 0000”. This is the
command for No Operation.
- 3.Give XTAL1 a positive pulse. This
loads the command, and the internal write signals are reset.
Figure 1. Addressing the Flash Which Is
Organized in Pages
Note: PCPAGE and PCWORD are listed in the
table of No. of Words in a Page and No. of Pages in the Flash in Page
Size section.
Programming the Flash
Waveforms
Note: “XX” is don’t care. The letters
refer to the programming description above.