AIN1 Digital Input
Disable
When this bit is written logic one, the digital input buffer on the
AINP1/0 pin is disabled. The corresponding PIN Register bit will always read as zero
when this bit is set. When an analog signal is applied to the AINP1/0 pin and the
digital input from this pin is not needed, this bit should be written logic one to
reduce power consumption in the digital input buffer.
AIN0 Digital Input
Disable
When this bit is
written logic one, the digital input buffer on the AINP1/0 pin is disabled. The
corresponding PIN Register bit will always read as zero when this bit is set. When
an analog signal is applied to the AINP1/0 pin and the digital input from this pin
is not needed, this bit should be written logic one to reduce power consumption in
the digital input buffer.