This section illustrates the GUI options available for the XC8 compiler in Microchip Studio.
XC8 Common Options
Option | Description |
---|---|
General Options |
|
-mrelax |
Controls the optimization of the long form of call and jump instruction |
Output File Options |
|
.hex |
Generate hex file |
.eep |
Generate eep file |
.usersignatures |
Generate usersignatures file |
.lss |
Generate lss file |
Miscellaneous Options |
|
Other Common Flags (Form field) |
Input other project-specific flags |
XC8 C Compiler Options
Option | Description |
---|---|
General Options |
|
-mcall-prologues |
Use subroutines for function prologues and epilogues |
-mno-interrupts |
Change stack pointer without disabling interrupts |
-funsigned-char |
The default char type is unsigned |
-funsigned-bitfield |
The default bit field is unsigned |
-nostdinc |
Do not search system directories |
-mext=cci |
Use CCI |
Symbol Options |
|
One can define (-D) or undefine (-U) and several in-source symbols. New symbol declarations can be added, modified or reordered, using the interface buttons below:
|
|
Include Directories |
|
Contains all the included header and definition directories, can be modified using the same interface as symbols. |
|
Optimization Options |
|
optimization level(drop-down menu): -O0,-O1, -O2, -O3, -Os, -Og |
No optimization, increasing general optimization (levels 1 & 2), optimize for speed (3), optimize for size, optimize for better debugging experience |
-ffunction-sections |
Prepare functions for garbage collection. If a function is never used, its memory will be scrapped. |
-fdata-sections |
Prepare data for garbage collection |
-fshort-enums |
Allocate only as many bytes needed by the enumerated types |
Debug Options |
|
Debug level (drop-down menu): none, g1, g2, g3 |
Specifies the level of tracing and debugging code and headers left or inserted in the source code |
Warning Messages Output Options |
|
-Wall |
Show all warnings |
-Werror |
Generation of errors instead of warnings for dubious constructs |
-pedantic |
Warnings demanded by strict ANSI C. Rejects all programs that use forbidden extensions. |
-w |
Inhibit all warnings |
Miscellaneous Options |
|
Other flags (Form field) |
Input other project-specific flags |
-v |
Verbose |
XC8 Linker Options
Option | Description |
---|---|
General Options |
|
-nodefaultlibs |
Do not use default libraries |
-Wl,-Map |
Generate MAP file |
-Wl,-u, -vfprintf |
Use vfprintf library |
Libraries Options |
|
Libraries -l (form field) |
You can add, prioritize or edit library names here using these buttons: , , , , |
Library search path -L (form field) |
You can add, prioritize or edit a path where the linker will search for dynamically linked libraries. It uses the same interface as above. |
Optimization Options |
|
-Wl,--gc-sections |
Garbage collect unused sections |
Miscellaneous Options |
|
Other Linker Flags (Form field) |
Input other project-specific flags |
XC8 Assembler Options
Option | Description |
---|---|
Miscellaneous Option |
|
Other Assembler Flags (Form field) |
Input other project-specific flags |
XC8 Archiver Options
Option | Description |
---|---|
General Options |
|
Archiver Flags (Form field) |
Input other project-specific flags |