The MPLAB® Data Visualizer is used to view live data and for debugging purposes.
It can display the following variables:
Moreover, debug messages, which display any faults or state changes, can be enabled and
viewed in the MPLAB Data Visualizer terminal section. The following lines of code are
contained in the application area of the project, in the app.c
file. It
is strongly recommended that only a single functionality is enabled at once, either the
debug messages or the Data Visualizer. Debug messages are disabled by default. To enable
them, comment lines 31 and 33 and uncomment line 30. Any changes to the code require
recompiling and reuploading the project.
.json
file in the root of the repository.app.c
source file macros), they can be
viewed in the Terminal tab, with the Display As mode set to 8-bit
ASCII