The motor will start without issues if a 24V supply voltage is provided and the default values are used.
However, the number of the pole pairs of the used motor may be different from the one used in the default configuration. If this is the case, normal behavior is exhibited, but the RPM seen in the MPLAB Data Visualizer will have an incorrect value.
To fix this issue, two fields in the AVR_Dx_tuning_params.xslm
excel
file need to be modified:
If the results are in order and the motor response is correct, then tuning is not necessary.