The following instructions describe how to install the MCC plugin and the I2C EEPROM AT24CM02
driver in MPLAB X IDE.
To install the MPLAB® Code Configurator Plugin:
- 1.In MPLAB X IDE, select Plugins from
the Tools menu.
- 2.Select the Available Plugins
tab.
- 3.Check the box for the MPLAB® Code Configurator and click on Install.
To install the I2C EEPROM AT24CM02 driver:
- 1.Open MCC in MPLAB® X
- 2.In the Content Type window, select MCC
Melody
- 3.Under Optional Content, go to Optional
Content → Libraries
- 4.Tick the box next to I2C EEPROM
AT24CM02 and click Finish
- 5.In the Content Manager window, select the latest or the preferred version of the driver in
Libraries → I2C EEPROM AT24CM02 and click Apply.