The easiest way to create a FreeRTOS application is to download an example from Atmel | START and work from there. This ensures that all FreeRTOS files will be included and working correctly. The demo code can then be removed, and the application development can begin.
In this application note, the following Atmel | START example project is used: ATmega4809 FreeRTOS Example.