Conversion during SLEEP mode when ADACQ=0 affects results on values in the upper half of the 10-bit range. The analog input is disconnected for 3-4 uS and the first bit of the result becomes zero.
Add 5 counts of ADACQ time.