The following is a list of the main components and interfaces on the AT32UC3L-EK:
Main MCU: Atmel AVR UC3 32-bit AT32UC3L064 (TQFP48)
64KB internal flash, 16KB internal RAM
Up to 50MHz operation
Very low power consumption
Capacitive touch module for support of QTouch and QMatrix capture from capacitive touch sensors
Peripheral event system
FlashVault™ allows pre-programmed, secure library support for end user applications
One touch rotor and five touch sensors
One 3-axis accelerometer (connected to channels 6, 7, and 8 of the ADCIFB module)
One serial data flash, 64Mb
One RTC 32kHz crystal
Four LEDs
One pushbutton
One reset pushbutton
Wireless expansion connector for the RZ600 AT86RF231 radio board PCBA or for y SPI-based, TWI-based, or USART-based external communication
36-pin raw expansion header for GPIO access
JTAG connector for programming and debugging on the AT32UC3L064 MCU
Powered through the USB connector, through an external power supply (header), or through a 1.2V battery (header J3)
USB (2.0 Mini-AB receptacle) connected to the 32-bit AVR UC3 AT32UC3B1256
AT32UC3L064 and AT32UC3B1256 are connected through two pins
One of the pre-loaded firmware on the AT32UC3B1256 acts as a UART-USB CDC virtual com port gateway
One of the pre-loaded firmware on the AT32UC3B1256 acts as UART-to-USB HID QTouch Debug interface to AVR QTouch Studio
USB mode pushbutton: with the default pre-loaded firmware on the AT32UC3B1256, the USB mode button is used to select between the UART-USB CDC virtual com port gateway firmware (press the USB mode upon power up of the board) and the UART-to-USB HID QTouch Debug interface to AVR QTouch Studio
The J12 jumper can be used to set the AT32UC3B1256 in boot loader mode at power up
JTAG connector for programming and debugging the AT32UC3B1256 (J13)