The Atmel® AT32UC3L-EK is an evaluation kit and development system for the Atmel AVR® UC3 AT32UC3L064 microcontroller.
As an evaluation kit, the board focus is towards Atmel QTouch® and QMatrix™ support, and Atmel picoPower® technology.
As a development system, the board notably provides on-board memory, a USB communication interface, an accelerometer, and the JTAG programming and debugging interface. The AT32UC3L-EK also features expansion headers; one of these is the wireless expansion header (named WLESS on the PCB), which is the receptacle for one of the two RZ600 radio boards provided in the kit package.