A few test points covering the user interface block have been placed on the AT32UC3L-EK for the verification of important signals.
Designation | Feature |
---|---|
TP1 | Input voltage on the AT32UC3L064 RESET_N pin, depending on the state of the RST pushbutton |
TP18 | Input voltage for the accelerometer. Should be 1.8V nominal |
TP15 | Output voltage on the accelerometer VoutZ pin |
TP16 | Output voltage on the accelerometer VoutY pin |
TP17 | Output voltage on the accelerometer VoutX pin |
TP19 | Input voltage on the AT32UC3L064 WAKE_N pin, depending on the state of the WAKE pushbutton |
TP20 | Voltage level on LED0 |
TP21 | Voltage level on LED1 |
TP22 | Voltage level on LED2 |
TP23 | Voltage level on LED3 |
To locate the test points mentioned here above, use the assembly top/bottom views provided within the AT32UC3L-EK schematics package.