Event generation and event actions are configurable in the ADC.
The ADC has two actions that can be triggered upon event reception:
The ADC can generate two events:
Window monitor
Result ready
If the event actions are enabled in the configuration, any incoming event will trigger the action.
If the window monitor event is enabled, an event will be generated when the configured window condition is detected.
If the result ready event is enabled, an event will be generated when a conversion is completed.
Note: The connection of events between modules requires the use of the SAM Event System Driver (EVENTS) to route output event of one module to the input event of another. For more information on event routing, refer to the event driver documentation.