The Oscilloscope control panel is where the oscilloscope is configured and connected to the rest of the system. The control panel has five sections, which are described in detail in the following sections.