This chapter gives an example on how to configure the
Graph module to be used with a target application
implementing a Night mode switch with a light sensor. Although this example utilizes
only some of the data sources available in the Data Visualizer, the procedure will be
the same for all data sources. The target code used in this example and a description of
the hardware setup can be found in the Graph Example Code chapter. The first part of the configuration example
uses the code found in the first subsection of the Graph Example Code chapter (Basic Graph). When changes to the target application code are
required as the example progress a link to the corresponding code listing will be
provided.
Todo: Select correct tool in the
DGI Control Panel.
Todo: Click
Connect to make a connection to the DGI on the selected
tool.
Todo:
- Click the
SPI checkbox
- Open the
SPI Configuration dialog by
clicking the Gear button next to the
SPI checkbox
Todo:
- Open the configuration
panel
- Add a
Graph module to the Data Visualizer
- Drag the
source connector from the interface in the
DGI Control Panel into the
sink marked New plot to
make a connection to a new plot
Todo:
- Push
Start in DGI Control
Panel
The data will be plotted in the Graph module. It could look something like the
picture below when hovering a hand above the light sensor.
The light sensor data can be used to
switch between Day and Night mode. For the Night mode switch to be useful,
the threshold when switching between the modes are important. The
Graph module contains a useful feature called
Band to mark when the plot data is within a
certain range. This can be used to simplify the selection of the mode switch
threshold.
Todo:
- Drag the interface
source to the New band
sink
To see that the Night mode switch is actually working and switching at the
right threshold, the string marker feature of the Graph module is
useful. In this example, the CDC USART interface of the target board is used to send a
string each time the mode is switched. These messages can then be shown in the graph as
string markers. The target application source code for this part of the configuration
example can be found in Adding String Markers.
Todo:
- Open the Serial
Port Control panel found under External
Connection in the Modules section of
the Configuration tab in Data Visualizer
Todo:
- Select the correct COM port
corresponding to the connected kit
- Set the serial port
parameters according to the application code
- Make sure the Open
Terminal option is not checked
Todo:
- Drag the serial port
source to the New string
sink
- Click
Connect in the Serial Port Control
Panel
String markers will appear as vertical lines with a square on top. By
double-clicking the square the string text will be shown. Note that there will naturally
be some delay from the ADC data values crosses the threshold until the string message
reaches the host computer. In addition, the timestamping of the data is added on the
host computer and the two serial interfaces are not synchronized. This results in a
misalignment of the string markers compared to the ADC values. DGI includes timestamping
functionality on the EDBG on the Xplained Pro and this can be enabled in the
DGI Control Panel at a performance cost, but CDC includes no
time stamping functionality.
Tip: In this example, a separate serial
interface was used for the string marker data. If the number of serial interfaces
available are constrained, the same interface could be used to stream both the ADC
data and the string marker data by using the Atmel Data Protocol (ADP). For more
information, see the
Atmel Data Protocol.
So far, the Graph
module of the Data Visualizer has been used to show the data generated by the light
sensor and to show when the Night mode switch toggles between the two modes. The
Graph module can also be used to interact with the target
application while it is running. In this example, the Night mode threshold can be
adjusted dynamically by using a horizontal cursor.
The target application source code for this part of the configuration example can be found
in Using Horizontal Cursor Code.
Todo:
- First, remove the band from
the graph as it is of no use when the Night mode threshold is dynamic
- Click Add Horiz.
Cursor to add a horizontal cursor to the graph
- Drag the
Horizontal Cursor
source to the sink in the
Serial Port Control Panel
To move the horizontal cursor either drag it or change the value by typing a new
value in the
Value field in the configuration. Note that the
value will not be updated until the
Value text box is not in
focus, i.e. click somewhere else in the GUI after typing in a value. Every time the
cursor is moved the Data Visualizer sends a new float value to the serial port the
cursor is connected to.
Tip: Turn off
Auto-scroll and Automatically fit Y to
more closely examine a plot while it is still running.