When using the Auto Labels mode each cell is associated with one data source and the name of the data source is shown to the left in the cell and the actual data to the right. The source name is automatically fetched from the source connected to the sink endpoint.
The Table element has one endpoint per table cell accepting any data source. The data will be converted to a string and displayed as text.