Parameter | Type | Usage |
---|---|---|
Font Size | Numeric | Sets the font size of the button tag |
Text | String | Sets the button tag text. If the button is configured as a toggle button the test should be delimited by '/'. The first part of the text will then be the ON state text while the second part will be the OFF state text. |
Toggle Button | Checkbox | Configures the button to be a ON/OFF toggle switch. |