Now see how components placed on a dashboard in Data Visualizer can be hooked up to variables in the application, and how the dashboard can thus interact with the application at run-time.
volatile uint32_t frame_comparator = 100; volatile uint32_t frames_received = 0; void ui_process(uint16_t framenumber) { frames_received++; if (frames_received >= frame_comparator) { LED_Toggle(LED_0_PIN); frames_received = 0; } }