This section gives an example on how to configure the
Dashboard module. Although the example utilizes only a subset
of the available dashboard elements data sources available in the Data Visualizer, the
basic principles are applicable to all elements and data sources.
This example uses manual configuration of the
Dashboard module, but it is also possible to use the Atmel
Data Protocol (ADP) to set up a dashboard automatically. For more information on ADP and
an example of a automatically configured dashboard, see Atmel Data Protocol.
The target application code used in this example and a description of the hardware setup can be found in Dashboard Example Code.
Todo:
- Open the configuration panel
- Add a new I/O Dashboard
component by double-clicking the I/O Dashboard module
Todo:
- Enable editing the dashboard
by clicking the Edit option in the lower left corner
of the Dashboard I/O module
- Open the
Elements panel in the upper right corner of the
dashboard and drag elements onto the dashboard.
Tip: To remove an element
from the dashboard, select it by left-clicking it, and then right-click the
element.
Tip: Changing the parameters
in the Configuration section will not take effect until the
Set button is clicked.
In this example, three
Label elements are added, one as a
title for the dashboard and the two others as help text for the slider. A
Graph element with one plot was added to be used for the
light sensor data. The
Y Minimum and
Y
Maximum values were set to 0 and 255, respectively. A
Signal element was added to be able to see which mode is
active. When the Night mode is active the signal turns dark blue (
Color
On) and when the Night mode is inactive the signal turns yellow
(
Color Off). Finally, a slider was added to make it possible
to adjust the Night mode threshold. The
Minimum was set to 0 and
the
Maximum was set to 255. Moving the slider to the left lowers
the threshold and results in the Night mode being active at brighter light levels.
When the dashboard has been set up it is time to connect the dashboard to the
serial interfaces to enable communication with the target application.
Before the endpoints in the dashboard can be
hooked up, the interfaces between the target board and the host
computer must be configured. This example uses the DGI SPI
interface and the CDC USART interface. The CDC interface will
appear on the host computer as an ordinary serial COM port.
Todo: Select correct tool in the
DGI Control Panel.
Todo: Click
Connect to make a connection to the DGI on the selected
tool.
Todo:
- Click the
SPI checkbox
- Open the
SPI Configuration dialog by
clicking the Gear button next to the
SPI checkbox
Todo:
- Open the Serial
Port Control panel found under External
Connection in the Modules section of
the Configuration tab in Data Visualizer
Todo:
- Select the correct COM port
corresponding to the connected kit
- Set the serial port
parameters according to the application code
- Make sure the Open
Terminal option is not checked
Todo:
- Deselect the
Edit option
- Click the Show
Endpoints option
- Drag the SPI
source to the graph
sink
- Drag the serial port
source to the signal
sink
- Drag the slider
source to the serial port
sink
Now the dashboard is fully configured and can be used
to interact with the Night mode switch application.
Todo:
- Deselect the Show
Endpoints option
- Click
Start in the DGI Control
Panel
- Click
Connect in the Serial Port Control
Panel
Now the ADC raw values are shown in the graph and the slider can be adjusted to a
suitable threshold for the Night mode switch. The signal element shows the state of the
switch.