An example on how to use Program Counter
sampling for power consumption analysis can be found in Program Counter Polling. The same Mass Storage Class example
used in this section is also suited as an example on how to use the data
polling and control of data variables features. A SAM L21 Xplained Pro board
is connected to a host computer both through Target USB and Debug USB
connectors on the kit. The ATSAML21 target device is running the USB Device
MSC Example from ASF for SAM L21 Xplained Pro.
For more information on the hardware setup and target application code used
in this example, see Data Polling Example Code.
Although this example makes use of the Graph and
Dashboard modules the principles are the same for using the
Code Profiling interface with the other modules in the Data
Visualizer.
First, a graph will be set up to monitor variables in the target
application.
Todo:
- Enable the Code
Profiling interface by deselecting the check box for the
Code Profiling interface in the DGI
Control Panel
Todo:
- Open the Code
Profiling Configuration window by pushing the Gear
button
Todo:
- Click the Add
Memory Location button for each memory location to be
added
- Fill in the address and
format of each location
Todo:
- Open the
Configuration panel in Data
Visualizer
- Add a
graph by double-clicking the
Graph module
A new Graph element will open with one y axis
configured. However, there are two unrelated variables to monitor, therefore, two axes
are needed.
Todo:
- Click the Add
axis button to add an additional axis
There are now sources (variables) and sinks
(axes), to be connected together.
Todo: Drag
each of the source plugs on the
Code Profiling interface into the
New plot
(sink) jack of each axis.
Todo: In
Atmel Studio click Continue (F5) to resume execution.
Tip: A USB device in the
HALT state no longer responds to Windows events, and may be disconnected from the
bus if held in this state for too long. To remedy this simply reset execution in
Atmel Studio.
Look at the output in the graph in Data Visualizer. Format the
disk and watch how the write cycles counter increments. Both values are plotted on
independent axes, so they can be scaled accordingly. The output should look something
like this:
The following part of this example shows how to use a dashboard to interact
with the target application. For more information on the required code changes in the
target application, see Application Interaction using Dashboard Controls.
Todo:
- Open Data Visualizer
- Connect
- Add the location of the
frame_comparator in the Code Profiling Configuration window
A Data Visualizer dashboard can now be made with controls which manipulate the
value of this variable.
Todo:
- Open the configuration panel
- Add a new I/O Dashboard
component by double-clicking the I/O Dashboard module
A slider control can now be added to the dashboard.
Todo:
- Select the Edit checkbox
- Open the Elements tab
- Drag a Slider element onto
the dashboard
A slider control needs to have some configuration
parameters.
Todo: Select the slider element and set
its properties:
- Maximum = 500
- Minimum = 100
A segment display control can now be added to the dashboard.
Todo:
- Select the Edit checkbox
- Open the Elements tab
- Drag a Segment Display
element onto the dashboard
A segment display control needs to have some
configuration parameters.
Todo: Select the segment display element
and set its properties:
The slider control can now be used as a source which can be connected to any
relevant sink in Data Visualizer. The segment display can similarly be used as a sink to
connect any relevant source to.
The Code Profiling data polling interface provides
both a source of data and a sink of data. The slider can now be connected to the sink
and the segment display to the source.
Todo:
- Deselect the Edit
checkbox
- Select the Show Endpoints
checkbox
- Connect sources to sinks by
dragging each source plug and drop it on a
sink
Now that the connections have been made in Data
Visualizer, the system can be put into a running state and interaction with the variable
can be made through the GUI.
Todo:
- Deselect the Show Endpoints
checkbox
- Start Data Visualizer
- Resume execution in Atmel
Studio (F5)
The slider is now in control of the frame_comparator variable in the application
code. Drag the slider, and notice that the LED blink frequency changes. Any change in
the slider position will be sent to the target device through the debug interface, and a
new value stored in the variable. At the same time, the value is also read back from the
target and displayed on the segment display.