The various dashboard element types are presented in this section. All element types have some common parameters. These are listed in the table below. The following sections will list only the parameters specific to each element type.
Parameter | Type | Usage |
---|---|---|
Z-index | Numeric | Order index, 0 places the element the farthest to the back |
Left | Numeric | Horizontal placement, unit pixels |
Top | Numeric | Vertical placement, unit pixels |
Width | Numeric | Width of element in pixels |
Height | Numeric | Height of element in pixels |