The SPI interface
source contains the raw
values received on the SPI interface. The
sink sends values received
back out on the SPI bus. For further details on the physical part of the SPI interface, see
the user guide of the debugging tool to be used to sample the SPI data.
Important: If the SPI
sink is connected to a source with a
multibyte type, the byte order may be unpredictable.
Important: The SPI hardware module uses an
active-low Chip Select (CS) signal. Any data sent when the CS pin is high will be
ignored.
The SPI Configuration dialog is opened from the
SPI interface in the DGI control
panel.
Table 1. Configuration
Field Name |
Values |
Usage |
Transfer Mode |
- SCK normally low, Read data on rising edge
- SCK normally low, Read data on falling edge
- SCK normally high, Read data on falling edge
- SCK normally high, Read data on rising edge
|
SPI mode, controlling clock phase and sampling. |
Force synchronization on CS |
ON or OFF |
The SPI interface is only enabled after the Chip Select line
has toggled twice. |
Enable timestamping |
ON or OFF |
Data is timestamped through the DGI timestamp interface
(yields a slower transfer rate). |