This example will block on each character sent via the OCD messaging system until it is ready to accept a new character. A simple timeout is employed to prevent full lockup of code if the debugger is disconnected. This example runs on an AVR ATtiny817 using the UPDI interface, but a similar mechanism could be used on other AVR MCU architectures supporting OCD messaging.
#include <avr/io.h> #include <stdbool.h> #define SYSCFG_OCDM SYSCFG.reserved_0x18 #define SYSCFG_OCDMS SYSCFG.reserved_0x19 bool ocd_print_ready (void) { // Has the last character been collected? return !(SYSCFG_OCDMS & (1 << 0)); } bool ocd_print_char (char msg) { // Simple timeout mechanism uint8_t timeout = 0xFF; while (timeout-- && !ocd_print_ready()) ; // If the debugger fails to collect, continue if (!timeout) return false; // Drop off a message SYSCFG_OCDM = msg; return true; } void ocd_print (char* pmsg) { // Send the message while (*pmsg) { if (!ocd_print_char(*pmsg++)) return; } } int main(void) { // Send an OCD message ocd_print ("Hello World\n"); while (1) ; }