A typical use of the Terminal module is print-type debugging. A serial interface is used to print debug messages from the target device to the terminal. In the following example an SPI interface will be used but the procedure will be the same for any serial interface.
The target device is an ATmega256RFR2 on an ATmega256RFR2 Xplained Pro kit. As the SPI interface is already wired internally on the board, the only connection needed is the USB cable between the host computer and the Xplained Pro board.
#include <avr/interrupt.h>
#include <avr/sleep.h>
volatile uint8_t led_on;
volatile uint8_t send_message;
volatile uint8_t ticker = 0;
const char* message_on = "LED ON ";
const char* message_off = "LED OFF ";
ISR (INT4_vect)
{
// Simple debounce
if (PINE & (1 << 4))
return;
// Update LED
if (led_on)
PORTB |= (1 << 4);
else
PORTB &= ~(1 << 4);
// Invert led_on
led_on = ~led_on;
// Flag a message send
send_message = 1;
// Increment ticker
ticker++;
// Reset ticker
if (ticker >= 10)
ticker = 0;
}
void spi_send (const char data)
{
PORTB &= ~(1 << PINB0);
// Send a character to the USART
SPDR = data;
// Wait for the character to be sent
while (!(SPSR & (1 << SPIF)))
;
PORTB |= (1 << PINB0);
}
int main(void){
// PORTB4 to output
DDRB = (1 << PINB4);
// LED OFF
PORTB |= (1 << PINB4);
led_on = 0;
// Enable pullup on button pin to avoid floating line
PORTE |= (1<<PINE4);
// Enable falling edge interrupt for button pin
EIMSK = (1 << INT4);
EICRB = (1 << ISC41);
// SPI
// MOSI, SCK and /SS as output
DDRB |= (1 << PINB2) | (1 << PINB1) | (1 << PINB0);
// Set /SS high
PORTB |= (1 << PINB0);
// Enable SPI, Master, set clock rate fck/16
SPCR = (1 << SPE) | (1 << MSTR) | (1 << SPR0);
// Interrupts on
sei();
while(1) {
if(send_message) {
// Send a message
const char* pmessage;
if (led_on)
pmessage = message_on;
else
pmessage = message_off;
while (*pmessage)
spi_send(*pmessage++);
// Send the ticker value
spi_send(ticker + '0');
spi_send('\n');
// Sent
send_message = 0;
}
}
}
The code triggers an interrupt when the switch (SW0) on the Xplained Pro board is pushed and toggles the LED0 at each push. Each time the switch is pushed a message is printed on the SPI interface.